PCE-VT 3900 Vibration Meter with Internal Memory
PCE Instruments’ vibration meter analyzes measured values and shows a corresponding good/bad rating on a display
PCE Instruments’ PCE-VT 3900 vibration meter is an ideal measuring device for fast and precise checking of vibrating parts, machines, and systems. The meter uses the external vibration sensor to determine the vibration displacement (measuring range 0.000 mm to 3.9 mm), the vibration velocity (measuring range 0.00 mm/s to 399.9 mm/s), and the vibration acceleration (measuring range 0.0 m/s² to 399.9 m/s²). Various measurement parameters, such as RMS, peak, peak-peak, and crest factor, are available for the vibration meter.
The PCE-VT 3900 vibration meter is equipped with a mode that allows a measurement to be automatically evaluated according to the limit values of ISO 10816-3. The vibration meter analyzes the measured values and shows a corresponding good/bad rating on the display. The built-in battery in the vibration measuring device has a capacity of 2500 mAh and can be recharged directly via the built-in micro USB interface.
In addition to the normal measuring mode, the vibration meter has an FFT mode. In FFT mode, the frequency spectrum for the measured vibration speed or acceleration is calculated and displayed. The calculated FFT lines are displayed in a graphic representation in an overall view for the entire frequency band and parallel to this in a zoomed view to display the individual lines.
An additional function is route measurement, which is specially designed for recurring measurements at identical measuring points. This enables an orderly measurement of different measuring points. Because of its extensive measuring functions, the vibration meter is used for maintenance and repair work on machines. The measurement data displayed for the various measurement functions can be stored in the internal memory of the vibration meter. After a measurement, the measurement data stored on the vibration meter can be transferred to a PC via the built-in micro USB interface. The software for the vibration meter then enables a graphic and tabular analysis of the measured values. The software can export the measurement data as a CSV file for further processing. In order to keep the vibration measuring device up to date, the software can also perform an automatic firmware update in addition to analyzing the measurement data.
- Acceleration: 0.0 m/s² to 399.9 m/s² (0.0 in./s² to 15,744 in./s²)
- Velocity: 0.00 mm/s to 399.9 mm/s (0.00 in./s to 15.74 in./s)
- Displacement: 0.000 mm to 3.9 mm (0.000 in. to 0.154 in.)
- Automatic ISO 10816-3 evaluation
- FFT analysis
- Data logger: 50 memory locations with 43,200 measured values each
- Route measurement
- Rechargeable battery
- Color graphic display
- Inspection of vibrations in machines and systems