Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
Mini Lug Temperature Sensors Slide 5

The Mini Lug Temperature Sensor electrical parameters are outlines in the Quick Reference Data table. As one can see, the Mini Lug Sensor provides designers with an array characteristics. First and foremost, the Mini Lug can be produced with different resistance vs. temperature (RT) curves. Depending on the curve, designers also have a choice of electrical resistance values at the reference temperature of +25°C (R25) to meet the self-heating, voltage output, or noise suppression needs of their application. The tolerance on the chosen R25 value could be as low as ±2%. The Mini Lug also provides accurate measurements over a wide temperature range from -40°C to +125°C. If standard characteristics do not fit an application, custom electrical and mechanical values are available upon request.

PTM Published on: 2011-06-14